In modern agriculture, accurate seed singulation and population counting are vital to achieving high crop yields and avoiding the significant cost penalties of missed seeds (skips), multiple seeds (doubles), and population errors. ROJ integrates edge AI directly into the seed metering unit with its Vision4Seeding platform, using the STM32N6 MCU to detect seed status in real time at 38 inferences per second. Operators get automated visibility on every row, with no cloud dependency.
 

Application domains:

  • Precision seed planting
  • Smart farming and AgTech
  • Agricultural machinery (OEM and retrofit)

Approach

As farms grow larger and the variety of crops increases, the whole industry shares the need for more precise seed planters. Accurate singulation, meaning exactly one seed placed at each position, directly impacts crop yield and farm economics.

Single seeds, doubles and skips on a seeding disc Single seeds, doubles and skips on a seeding disc Single seeds, doubles and skips on a seeding disc

Traditional solutions struggle to meet these demands, especially in multi-row, high-speed operations with diverse seed types. On planters with over 40 rows and discs spinning at 30 to 40 rpm, the task becomes significantly more complex. Seed sensors on tubes fail with small or irregular seeds and often miss or double-count. Cameras on seeding discs often deliver low-resolution or blurred images at high seeding speeds, and still rely on the operator's eye and manual adjustments. Both approaches fall short of the precision modern agriculture requires.

Grid of low-resolution, blurred camera views of spinning seeding discs Grid of low-resolution, blurred camera views of spinning seeding discs Grid of low-resolution, blurred camera views of spinning seeding discs

Vision4Seeding changes this by integrating edge AI directly into the metering unit. Machine vision algorithms running on the STM32N6 continuously analyze high-speed camera feeds from each planter row, detecting skips and doubles and counting seeds in real time.

 

Key benefits of this edge AI approach:

  • Automated real-time monitoring: AI continuously detects planting errors, so operators no longer need to watch camera feeds
  • High precision and consistency: Errors are detected even at higher RPM, independent of lighting and operator fatigue
  • No cloud dependency: Inference runs on the device, minimizing latency and network requirements
  • Bandwidth-efficient: Only relevant snapshots and compact inference results are sent to the operator interface
  • OEM and retrofit compatible: A flexible path for both new and existing machinery

Application overview

The Vision4Seeding system integrates a global shutter camera with dedicated illumination, mounted directly on the metering unit.

Vision4Seeding camera unit mounted on a planter's seed metering unit Vision4Seeding camera unit mounted on a planter's seed metering unit Vision4Seeding camera unit mounted on a planter's seed metering unit

1. Synchronized image capture

Each cycle begins with a synchronization signal from the seeding disc, which triggers image capture so that the new seeds are in frame.

2. Real-time edge inference

Snapshots are processed in real time by an optimized neural network on the STM32N6, accurately detecting seeds, skips, and doubles even at high speeds and across diverse seed types.

3. Result transmission and monitoring

Snapshots are compressed to JPEG and sent, together with the inference results, via Ethernet to the operator interface for centralized monitoring of multi-row planters. Sending only relevant images and compact inference data ensures precise visibility while minimizing bandwidth usage.

“

Powered by the STM32N6 MCU's advanced AI acceleration, Vision4Seeding gives the operator a superpower: AI now sees every seed status in real time. No more staring at camera feeds. With high-performance, low-latency inference at the edge, operators can focus on driving while Vision4Seeding guarantees perfect singulation.

”

Luca Bagatin, R&D Manager at ROJ

Technical details

Vision4Seeding relies on the AI acceleration of the STM32N6 (Neural-ART NPU) to run object detection on every capture cycle. With an inference time of 26 ms, the system sustains 38.4 inferences per second, keeping pace with high-speed planting operations where the disc spins rapidly and image capture must stay synchronized with disc rotation.

Sensor

Global shutter color sensor: VD66GY

The VD66GY captures sharp, coherent color images at high speed, avoiding motion distortion even when the seeding disc is spinning rapidly. This ensures reliable input for the detection model across operating speeds.

Model and results

Model:

  • Object detection (seeds, skips, doubles)
  • Architecture: ROJ custom lightweight neural network for seed detection
  • Parameters: 0.99 M
  • Input size: 320 × 320 × 3

Results:

  • Weights (Flash): 943.25 KB
  • Activations (RAM): 1.848 MB
  • Inference time: 26 ms
  • Inferences per second: 38.4
  • Object detection mAP@0.5 (on board): 0.859
Dataset tool showing seeding disc images with labeled and predicted seed positions Dataset tool showing seeding disc images with labeled and predicted seed positions Dataset tool showing seeding disc images with labeled and predicted seed positions

Software tools

Documentation

Optimized with

STM32Cube AI Studio

STM32Cube AI Studio

Most suitable for

STM32N6 Series

Most suitable for

Resources

Optimized with STM32Cube AI Studio

STM32Cube AI Studio is a desktop tool designed to evaluate, optimize and compile neural network models for STM32 microcontrollers. It fully supports compilation for the Neural-ART Accelerator neural processing unit (NPU). It replaces the X-CUBE-AI in the ST AI product offering to cover new STM32 devices.

Optimized with STM32Cube AI Studio Optimized with STM32Cube AI Studio Optimized with STM32Cube AI Studio

Most suitable for STM32N6 Series

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

Most suitable for STM32N6 Series Most suitable for STM32N6 Series Most suitable for STM32N6 Series
You might also be interested by

Industrial | Current sensor | STM32Cube AI Studio | Model zoo | STM32 AI MCU

How to make solar inverters safer with AI arc fault detection

The STM32H7P runs AI arc fault detection on 20 solar inverter channels in a single chip, learning from field data instead of hand-tuned rules.

Vision | STM32 AI MCU | Partner | Video | Industrial | STM32Cube AI Studio | Microphone | Appliances

How edge AI is redefining clear speech in a noisy world

Real-time audio denoising on STM32N6 with no DSP, delivering low-latency clean speech in noisy environments using edge AI.

Vision | STM32 AI MCU | Partner | Video | Smart city | Industrial | Smart home | STM32Cube AI Studio

People counting and tracking in retail environments

embedUR delivers real-time person segmentation on STM32N6 using YOLACT, achieving on-device people counting at 14 FPS with no cloud dependency.