Understanding these parameters is essential to select the right current sensor for your application and to optimize system performance.
Accuracy
Defines how close the sensor’s output is to the true value of the current being measured. It includes all sources of error such as offset, gain error, linearity error, and noise.
Importance:
- Determines the reliability of current measurement.
- Critical in applications requiring precise current monitoring, such as battery management and power metering.
Factors affecting accuracy:
- Input offset voltage and drift.
- Gain error and gain drift.
- Temperature variations.
- Noise and interference.
Bandwidth & Slew rate
Is the range of frequencies over which the sensor can accurately measure current without significant attenuation or phase shift.
Importance:
- Defines the sensor’s ability to track rapid changes in current.
- Important for dynamic applications like motor control or switching power supplies.
Typical values:
- Low bandwidth (~kHz) for slow-changing currents. for DC measurement, such as BMS applications
- High bandwidth (hundreds of kHz to MHz) for fast transient detection. AC measurement or motor control applications
Linearity
Describes how well the sensor’s output fit line relationship with the input current over its measurement range.
Importance:
- Ensure proportional and predictable output.
- Non-linearity causes distortion and measurement errors.
Measurement:
- Expressed as a percentage of full-scale output.
- Typical values are less than 0.1% for high-precision sensors.
Offset and Drift
Offset: the output signal when the input current is zero.
Offset: the output signal when the input current is zero.
- Ideally zero, but practical sensors have a small offset voltage.
Drift: variation of the offset with changing temperature or time.
- Causes measurement errors if not compensated.
Importance:
- Low offset and drift improve measurement accuracy, especially at low currents.
- Zero-drift amplifiers and temperature compensation techniques reduce these effects.
Summary table of key parameters of current sensing
| Definition | Importance | Typical Impact |
|---|---|---|---|
| Accuracy | Closeness to true current value | Critical for reliable measurement | Affects overall measurement quality |
| Bandwidth | Frequency range sensor can track | Needed for dynamic current sensing | Limits response to fast changes |
| Linearity | Proportionality of output to input gives information how the gain error is constant through the linear input range | Ensures predictable output | Non-linearity causes distortion affect accuracy measurment |
| Offset & Drift | Output at zero input and its variation over time/temperature | Impacts low current accuracy | Causes baseline errors |
Summary table of key parameters of current sensing
| Definition | Importance | Typical Impact |
|---|---|---|---|
| Accuracy | Closeness to true current value | Critical for reliable measurement | Affects overall measurement quality |
| Bandwidth | Frequency range sensor can track | Needed for dynamic current sensing | Limits response to fast changes |
| Linearity | Proportionality of output to input gives information how the gain error is constant through the linear input range | Ensures predictable output | Non-linearity causes distortion affect accuracy measurment |
| Offset & Drift | Output at zero input and its variation over time/temperature | Impacts low current accuracy | Causes baseline errors |