Making buildings smarter to improve their efficiency is one of the biggest challenges companies have to face. The people flow counting sensor developed by Schneider Electric in partnership with STMicroelectronics enables the counting of the number of people. It also detects whether they are crossing a virtual line in both directions, using a large field of view and a small resolution thermal sensor.

This promising technology opens a new solution for attendance monitoring and people counting in numerous applications such as monitoring queues, building usage, and social distancing. Our innovative demonstration, created with STMicroelectronics, finds applications in various segments, from hotels to offices and retail, and more generally any building where knowing attendance and space occupation has a value. This will redefine the building of the future!

Maxime Loidreau, IoT Sensors Program Manager at Schneider Electric

Approach

- This prototype can count in real-time and with a high level of accuracy the restaurant's attendance, while running on the standard STM32 microcontroller.
- This is achieved thanks to the artificial intelligence algorithm embedded on the STM32 microcontroller and the use of a thermal infrared technology.

Sensor

LYNRED thermal infrared camera
Code optimized with
STM32Cube.AI
STM32Cube.AI
Running on
STM32H7 series
STM32H7 series

Resources

Code optimized with STM32Cube.AI

A free STM32Cube expansion package, X-CUBE-AI allows developers to convert pretrained AI algorithms automatically, such as neural network and machine learning models, into optimized C code for STM32.

STM32Cube.AI STM32Cube.AI STM32Cube.AI

Running on STM32H7 series

The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor is designed to offer new degrees of freedom to MCU users. It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

STM32H7 series STM32H7 series STM32H7 series
You might also be interested by

Vision | STM32Cube.AI | STM32 AI MCU | Partner | Video | Smart home | Smart building

How to personalize smart home with familiar face identification

embedUR's on-device face authentication embedded on STM32N6 with easy mobile enrollment

Vision | STM32Cube.AI | STM32 AI MCU | Partner | Smart home | Wearables | Microphone | Accelerometer | Tutorial

Handheld development platform for real-time vision, motion, and voice at the edge

All‑in‑one STM32N6‑based platform for on‑device edge AI with NPU acceleration

Industrial | Smart city | Vision | STM32Cube.AI | STM32 AI MCU | Partner | Video | Smart home

Secure entry systems using id3 face recognition with liveness detection

Edge processing with RGB camera and ToF sensor ensures rapid and secure anti-spoofing for access control using the STM32N6 MCU.