Loading spinner

Silicon photonics

Enabling the future of cloud optical interconnects for faster and more efficient data transfers in datacenters and AI clusters 

ST is at the forefront of enhancing digital infrastructure, addressing the growing demands of AI and high-speed data communication. Silicon photonics (SiPho) technology leverages silicon-based materials to develop photonic circuits, which use light to transmit data. Silicon photonics is a highly promising technology for faster and more efficient data transfers in optical modules.

Close-up of a fiber optic cable connector with yellow and green cables Close-up of a fiber optic cable connector with yellow and green cables Close-up of a fiber optic cable connector with yellow and green cables

Pluggable optical transceivers accelerate data exchanges

Optical transceivers embedded in pluggable optics play a crucial role in converting optical to electrical signals and vice versa. They facilitate data flows between computing resources, switches, and storage devices, as well as transfers between servers, and between data centers.

ST’s proprietary silicon photonics technology, with its first photonic integrated circuit, the PIC100, offers a comprehensive design platform enabling a 200 Gbps per lane capability. This technology is tailored to meet the challenges of data speed, power efficiency, compactness, volume, and cost efficiency for the next generations of pluggable optical solutions delivering 800 Gbps and 1.6 Tbps.

Silion Photonics cloud optical interconnects Silion Photonics cloud optical interconnects Silion Photonics cloud optical interconnects

Powering the future of cloud optical interconnects 

ST unveils new silicon photonics and next-gen BiCMOS proprietary technologies.

Whitepaper the winning portfolio for AI optical interconnects Whitepaper the winning portfolio for AI optical interconnects Whitepaper the winning portfolio for AI optical interconnects

The winning portfolio for AI optical interconnects

Read more technical insights on silicon photonics and BiCMOS technologies for cloud optical interconnects.

Remi El-Ouazzane portrait Remi El-Ouazzane portrait Remi El-Ouazzane portrait

Driving the future of AI data centers with ST technologies

An interview with Remi El-Ouazzane, President, Microcontrollers, Digital ICs and RF products Group.

ST to drive EU-funded STARLight project 

Leveraging 300mm silicon photonics as the leading technology platform for application-based innovations built in the EU.

Silicon photonics wafer 300mm Silicon photonics wafer 300mm

A state-of-the-art design platform for better performance and higher energy efficiency in optical transceivers

High bandwidth

The technology platform supports bandwidth performance for modulators and photodiodes beyond 50 GHz and 80 GHz respectively.

Innovative technology stack for high energy efficiency

The patented technology stack features silicon and silicon nitride wave guides with very low sub-dB loss, as well as a low-loss edge coupling capability.

Future heterogeneous material integration

ST’s silicon photonics technology can combine heterogeneous components for developing even faster modulators. It can also enable semiconductor optical amplifier (SOA) and laser integration.

These advancements pave the way for 400 Gbps per lane modules for future 3.2 Tbps pluggable optics. 

A new range of compact modulators are under development to address a new class of optical links in AI clusters, which will reduce the congestion caused by the multitude of copper cables present today in AI cluster racks. The compact design of silicon photonics circuits and their integration in co-packaged optics are enabling the miniaturization of electro-optical devices. The transition of scale-up links from copper cable to optics will accelerate the deployment of AI clusters, supporting future growth.

The role of TSV technology in advancing silicon photonics 

Through-silicon via (TSV) is a critical enabler for the advancement of silicon photonics and co-packaged optics (CPO). This technology provides direct vertical interconnections in the silicon substrate to integrate photonic and electronic components more efficiently.

The high density in vertical interconnections provided by TSV, combined with the high-speed data transmission capabilities of silicon photonics, opens the door to more efficient and more compact systems. 

Silicon photonics and BiCMOS:
the backbone of hyperscalers

The combination of ST’s next-generation BiCMOS and silicon photonics technologies enables 800 Gbps and 1.6 Tbps solutions for hyperscalers.

  • ST’s silicon photonics technology brings customers the ability to integrate multiple complex components into one single chip.
  • ST’s BiCMOS technology provides exceptional cutoff frequency and gain for high-speed analog circuits, making it ideal for the critical blocks in optical transceivers.

These proprietary technologies provide better performance and energy efficiency to optical interconnects.

Server racks with illuminated lights in a data center Server racks with illuminated lights in a data center

Advanced in-house
manufacturing process

Silicon photonics and BiCMOS technologies are produced in ST's 300 mm production facility in Crolles, Europe, using advanced lithography to achieve high production yields in the category of digital CMOS. A global integrated device manufacturer (IDM), ST manufactures the entire value proposition in-house to ensure an independent high-volume supply for customers.

Technicians in cleanroom suits operating computers in a controlled environment Technicians in cleanroom suits operating computers in a controlled environment Technicians in cleanroom suits operating computers in a controlled environment